AKD-C Display Codes
During drive operation the drive display shows these codes depending on the drive status.
The AKD-C has one LED.
All codes with more than one character are displayed sequentially.
Display Code |
Status |
---|---|
|
No system power (inrush opened). |
|
Strings not fully powered (inrush closed). AKD-Ns cannot be enabled. The AKD-C has a fault which disables the AKD-Ns and unpowers the strings. |
|
Strings powered and drives disabled. AKD-Ns cannot be enabled. The AKD-C has a fault which only disables the AKD-N's control board temperature. |
|
Strings powered and drive operational. All AKD-Ns can be enabled. The AKD-C has no faults and strings are fully powered. |
+ [3 digit code, flashing] |
Fault (see Fault and Warning Messages). |
+ [3 digit code, flashing] |
Warning (see Fault and Warning Messages). |
+ [IP address] |
Displaying drive IP address. |
|
Powered on and FPGA loading. If the display is locked on this code, the operational and resident FPGA images are corrupt. |
|
Drive enabled. |
|
Download code. |
|
Special mode: Burn-in. |
|
Kernel error. |
|
Resident loading. |
|
Resident completed and waiting for the operational to start. |